SBOK110 June   2025 SN55LVTA4-SEP

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Overview
  5. 2Single-Event Effects (SEE)
  6. 3Test Device and Test Board Information
  7. 4Irradiation Facility and Setup
  8. 5Results
    1. 5.1 Single-Event Latch-up (SEL) Results
    2. 5.2 Single-Event Transients (SET) Results
  9. 6Summary
  10. 7References

Single-Event Latch-up (SEL) Results

During SEL characterization, the device was heated using forced hot air, maintaining device temperature at 125°C. A FLIR (FLIR ONE Pro LT) thermal camera was used to validate die temperature to make sure the device was accurately heated (see Figure 4-2.) The species used for SEL testing was a Xenon (129Xe) ion at 25MeV / µ with an angle-of-incidence of 0° for an LETEFF of 50MeV-cm2/ mg. A fluence of approximately 1 × 107 ions / cm2 was used for each run.

The three devices were powered up and exposed to the heavy-ions using the maximum recommended supply voltage of 3.6V using a National Instruments™ PXI Chassis PXIe-4139 on VCC and input 1A and a 3.6V, 10MHz square wave on input 4A using a National Instruments™ PXI Chassis PXIe-5423 function generator. The run duration to achieve this fluence was approximately 100 seconds. As listed in Table 5-2, no SEL events were observed during the eight runs, indicating that the SN55LVTA4-SEP is SEL-free. Figure 5-1, Figure 5-2, and Figure 5-3 show the plots of current versus time for runs one, three, and six, respectively.

A single unit was tested with a fluence of 1.5E+07 using the same bias condition as above. No SEL events occurred on these runs either.

Table 5-1 Summary of SN55LVTA4-SEP SEL Test Conditions and Results
Run NumberUnit NumberDistance (mm)Temperature
(°C)
IonAngleFlux
(ions × cm2 / mg)
Fluence
(Number of ions)
LETEFF
(MeV × cm2/mg)
Did an SEL Event Occur?
1170125Xe1.00E+051.00E+0750No
2

1

70125Xe1.00E+051.00E+0750No
3

2

70125Xe1.00E+051.00E+0750No

4

2

70125Xe1.00E+051.00E+0750No

5

3

70125Xe1.00E+051.00E+0750No

6

3

70125Xe1.00E+051.00E+0750No

7

4

70

125

Xe

1.00E+051.50E+07

50

No

8

4

70

125

Xe

1.00E+051.50E+0750No
 Current Versus Time for Run 1 of the
                    SN55LVTA4-SEP at T = 125°CFigure 5-1 Current Versus Time for Run 1 of the SN55LVTA4-SEP at T = 125°C
 Current Versus Time for Run 3 of the
                    SN55LVTA4-SEP at T = 125°CFigure 5-2 Current Versus Time for Run 3 of the SN55LVTA4-SEP at T = 125°C
 Current Versus Time for Run 6 of the
                    SN55LVTA4-SEP at T = 125°CFigure 5-3 Current Versus Time for Run 6 of the SN55LVTA4-SEP at T = 125°C

No SEL events were observed, indicating that the SN55LVTA4-SEP is SEL-immune at LETEFF = 50MeV-cm2 / mg and T = 125°C. Using the MFTF method shown in Single-Event Effects (SEE) Confidence Internal Calculations , the upper-bound cross-section (using a 95% confidence level) is calculated as:

Equation 1. σSEL≤6.15×10-8cm2/device for LETEFF=50 MeV∙cm2/mg and T=125℃