SBOS293J December 2003 – March 2025 OPA695
PRODUCTION DATA
A current-feedback operational amplifier such as the OPA695 holds an almost constant bandwidth over signal gain settings with the proper adjustment of the external resistor values. Section 5.9 shows this feature. The small-signal bandwidth decreases only slightly with increasing gain. These curves also show that the feedback resistor has been changed for each gain setting. The absolute values of RF on the inverting side of the circuit for a current-feedback operational amplifier can be treated as frequency response compensation elements, whereas the ratios of RF and RG set the signal gain. Figure 7-1 shows the analysis circuit for the OPA695 small-signal frequency response.
Figure 7-1 Current-Feedback Transfer Function
Analysis CircuitThe key elements of this current feedback operational amplifier model are:
A current-feedback operational amplifier senses an error current in the inverting node (as opposed to a differential input error voltage for a voltage-feedback operational amplifier) and passes this error current on to the output through an internal frequency-dependent transimpedance gain. Section 5.9 shows this open-loop transimpedance response. This response is analogous to the open-loop voltage gain curve for a voltage-feedback operational amplifier. For additional understanding on the CFA operating theory, see also the training videos at the TI Precision Labs.
The values for RF versus gain shown in Figure 7-2 are approximately equal to the values used to generate the typical characteristics and give a good starting point for designs where bandwidth optimization is desired.
Figure 7-2 Recommended Feedback Resistor vs Noise
Gain