SBOSAD1A May 2024 – July 2025 INA791A
PRODUCTION DATA
The typical error sources that have the largest effect on the total error of the device are gain error, nonlinearity, common-mode rejection ratio, and input offset error. For the INA791x, an additional error source (referred to as the reference voltage rejection ratio) is also included in the total error value.