SBOU126A April 2012 – October 2026 INA3221 , INA3221-Q1
INA3221EVM Default Jumper Settings shows the default jumper configuration for the INA3221EVM. Some of the jumpers on the INA3221EVM board can be changed to match specific configuration requirements. For example, a specific I2C address can be set by configuring jumpers J1 and J2.
Figure 2-8 INA3221EVM Default Jumper SettingsJumper 3 on the INA3221EVM is typically set to the INT position. When set to the INT position, the INA3221 supply voltage is generated and controlled by the SM-USB-DIG platform. When this jumper is set to the EXT position, VS connects to terminal strip T2.
Jumpers J1 and J2 control the INA3221 I2C address pin. These jumpers can set the address (A0) pin to either high, low, SCL, or SDA. Make sure to only connect one jumper at a time, never both. Failure to properly connect jumpers can cause shorts or interruptions in the communication lines. For more information on the INA3221 addressing, refer to the INA3221 product data sheet.
Table 2-2 summarizes the function of the INA3221 test board jumpers. For most applications, all jumpers must be left in the respective default configurations.
| Jumper | Default | Purpose |
|---|---|---|
| J1 | GND | These jumpers select the I2C A0 address selection. Four separate I2C addresses can be selected, depending upon whether J1 is set high or low or whether J2 is set to SDA or SCL. |
| J2 | Open | |
| J3 | INT | This jumper selects whether the INA3221 DVDD pin is connected to the VDUT signal generated from the SM-USB-DIG platform or whether the digital supply pin is connected to terminal T2, allowing for an external supply to power the digital circuitry. The default INT position connects the DVDD pin to the VDUT control signal. |