SCDA060 May 2025 CD4053B
An equivalent model can be built to describe the OFF-state leakage and make this easier for understanding and calculation. Both the OFF-state transistors and reverse-biased diodes can be regarded as large resistors, as shown in Figure 2-7. Other resistance for example, line resistance is neglected for simplification in this case.
From the output side, most of the leakage from input is sunk by the mid-point of transistors and cannot be seen at the output. Therefore, the paths linked to input can be removed as in Figure 2-8.
The paths linked to the same pin (VDD/VSS) can be combined and the final equivalent resistor model is shown in Figure 2-9.
To calculate the value of equivalent resistors Roff,up and Roff,down, connect the output to VDD and VSS respectively, and measure the current flowing out of the output.
The Roff,up and Roff,down can be calculated as the following:
Due to the symmetry of channel structure, a reasonable assumption is that Roff,up and Roff,down are of the same order of magnitude, for example, if Roff,up is tens of MΩ, Roff,down can also be assumed to be tens of MΩ.