SCDS384B September 2018 – August 2025 TMUX6119
PRODUCTION DATA
Off isolation is defined as the voltage at the drain pin (D) of the TMUX6119 when a 1-VRMS signal is applied to the source pin (SA or SB) of an off-channel. Figure 7-9 shows the setup used to measure off isolation. Use to Equation 2 compute off isolation.
Figure 7-9 Off Isolation Measurement Setup