SCES874A March 2017 – August 2026 SN74LVC1G79-Q1
PRODUCTION DATA
A useful application for the SN74LVC1G79-Q1 is using it as a data latch with low-voltage data retention. This application implements the use of a microcontroller GPIO pin to act as a clock to set the output state and a second GPIO to provide the input data. If the SN74LVC1G79-Q1 is being powered from 1.8V and there is concern that a power glitch could exist as low as 1.5V, the device will retain the state of the Q output. An example of this data retention is shown in Figure 7-2 where the VCC drops to 1.5V and the Q output maintains the HIGH output state when VCC returns to 1.8V. If the VCC voltage drops below 1.5V, data retention is not guaranteed.