SCEU029B August 2024 – June 2026
Use the P2 header block to interface the TPLD1202-RWS-EVM with an external system. Using the guide printed on the EVM silkscreen, interface the TPLD pins with an external system to allow for prototyping and testing in customer systems. When supplying power to the TPLD using the P2 header block, SW4 must be in the OFF position and a shunt placed on J1, connecting the external VCC supply from P2 (VCC_EXT) to the VCC net of the EVM. TI recommends not connecting the board to an external system and to the TPLD-PROGRAM at the same time to avoid the risk of damage to the TPLD-PROGRAM and the external system.
Figure 2-1 P2 and J1
Headers