SCEU029B August 2024 – June 2026
The TPLD1202-RWS-EVM can program both TPLD1202RWS and TPLD1202RWB without any changes to the board. To program a TPLD1202RWB, insert a TPLD1202RWB device into the RWS/RWB socket following the instructions in Section 3.2.2. Using the TPLD1202-RWS-EVM, select the TPLD1202RWB design and ICS, and configure normally, as described in Section 3.2.
Figure 3-8 RWS/RWB SocketWhen evaluating a TPLD1202RWB or TPLD1202RWS device, the IO map printed on the EVM is correct, but the pin numbers map to the incorrect pins of the device as the map corresponds to the pins of the TPLD1202RWS or TPLD1202RWS. Use this chart to determine the correct pin number for the RWB device from the markings on the board.
|
Pin Name |
RWS Pin Number |
RWB Pin Number |
|---|---|---|
|
IO1 |
3 |
5 |
|
IO2 |
4 |
6 |
|
IO3 |
5 |
7 |
|
IO4 |
6 |
8 |
|
IO5 |
8 |
10 |
|
IO6 |
9 |
11 |
|
IO7 |
10 |
12 |
|
IO8 |
11 |
1 |
|
IO9 |
12 |
2 |
|
GPI |
2 |
4 |
|
VCC |
1 |
3 |
|
GND |
7 |
9 |