SCEU029B August 2024 – June 2026
This user’s guide contains support documentation for the TPLD1202RWS and TPLD1202RWB evaluation module (EVM). Included is a description of how to set up and configure the EVM, how to use the EVM in conjunction with a TPLD-PROGRAM board, and how to use InterConnect Studio to configure the TPLD1202. Also included are the printed circuit board (PCB) layout, the schematic, and the bill of materials (BOM) of the TPLD1202-RWS-EVM.
The TPLD1202RWS and TPLD1202RWB are part of the TI Programmable Logic Device (TPLD) family of devices that feature versatile programmable logic ICs with combinational logic, sequential logic and mixed-signal functions to provide an integrated, compact, low power design to implement common system functions, such as timing delays, voltage monitors, system resets, power sequencers, and I/O expanders.
TI only supports the use of the cables provided in the TPLD-PROGRAM kit to interface between the EVM and the programmer board.