SCLA082 April   2025 TPLD1202 , TPLD1202-Q1 , TPLD2001 , TPLD2001-Q1

 

  1.   1
  2. 12
  3.   Trademarks

Application Description

Pulse-width modulation (PWM) is a method of providing a square or rectangular wave signal with a varying duty cycle commonly used in applications such as power conversion or controlling LED brightness. Some TI Programmable Logic Devices (TPLD) offer integrated pulse-width modulation generators that allow a designer to easily generate and control a square wave with variable duty cycle. This document provides an overview of the PWM generators included in the TPLD1202, namely what the available settings are and how to configure them in InterConnect Studio (ICS).

PWM Generator Components

When instantiated in ICS, the PWM generator (pwm0) appears alongside a counter module (cnt0) in Finite-State Machine (FSM) mode, as well as an internal oscillator (osc0), as shown in Figure 1.

 PWM Generator in ICS Figure 1 PWM Generator in ICS

The internal oscillator is automatically set to act as the clock to both the counter and PWM generator. The internal oscillator has settings that allow for a change in output frequency. You can also divide the frequency by changing the clock source setting on either the counter or PWM generator; the clock source setting also allows for use of an external clock source if desired. Note that to avoid output distortions, the counter and PWM generator uses the same clock source and operates at the same frequency. Configuration of the oscillator module is described in more detail in Utilizing Timing Components in TPLD.

Counter FSM Functionality

By default, the counter FSM works by counting down one value from the Control Data value for every clock pulse received until the internal count value is zero, at which point FSM provides an output pulse for one clock cycle, then resets. Figure 2 shows an example ICS counter simulation where the Control Data was set to 3 as seen in the counter settings shown in Figure 3; note that the counter (yellow) pulses high every three clock cycles (blue).

 Counter Module Settings Figure 2 Counter Module Settings
 Counter Simulation With Control Data of 3 Figure 3 Counter Simulation With Control Data of 3

The DATA connection shown in Figure 1 is the counter providing current internal count value to the PWM generator. This value determines the duty cycle of the PWM generator outputs. The duty cycle of the PWM signal can be calculated by: Duty cycle (%) = (DATA / 256) × 100, with a minimum duty cycle of 0% (0/256) and a maximum of 99.61% (255/256). Each change in count value provides an additive 0.39% increase or decrease in duty cycle.

The counter input signals UP, and KEEP as seen in Figure 1 exist when the Enable FSM Mode setting, visible in Figure 2, is selected for a given counter (counters providing DATA to a PWM are locked in FSM mode). These signals can be used to control the internal count value/DATA provided by the counter and thus dynamically change the duty cycle of the PWM generator. A logic high on UP causes the counter to count up to 255 before emitting a pulse, instead of down to 0. A logic high on KEEP maintains the current internal count value, regardless of any incoming clock pulses. A logic high on the RST input resets the current internal count value to the initial value set by the Control Data setting.

Figure 4 shows an ICS simulation of a counter with the various FSM signals employed. From top to bottom, blue is the clock, yellow is the counter output, green is the KEEP input, red is the RST input, and purple is the UP input.

 Counter FSM Simulation With Control Data of 3 Figure 4 Counter FSM Simulation With Control Data of 3

PWM Generator Configuration

In addition to the CLK and DATA connections, the PWM generator has a PUP (power-up) input that must be a logic high for the generator to provide an output signal, and two outputs OUT+ and OUT- that are in-phase with each other by default, as seen in Figure 1. The PWM configuration options are shown in Figure 5.

 PWM Configuration Options Figure 5 PWM Configuration Options

Both OUT+ and OUT- can be inverted by checking the appropriate Output Inversion box. A deadband of 0, 1, 2, or 5 clocks can be selected for OUT-; this setting reduces potential for shoot-through current when the PWM is used on circuits such as an H-bridge. A simulation waveform of the PWM generator with DATA of 128 (50% duty cycle), inverted OUT- output, and 5-clock deadband is shown in Figure 6. OUT- is blue and OUT+ is yellow. One full output period takes 255 clock cycles and is determined by the PWMs input clock source.

 PWM Simulation Figure 6 PWM Simulation

Example Circuit

The circuit in Figure 7 is configured to dynamically vary the PWM generator's duty cycle in an example overvoltage and undervoltage detection and control application. The PWM is set to run at 50% duty cycle by default (cnt0 is given a control data of 128), with KEEP set to be a logic high. The multi-channel analog comparator (mcacmp0) is used to detect voltages below 800mV and above 1.216V. When a voltage above 1.216V is detected, KEEP is set low and the counter is allowed to count down to decrease the duty cycle until the voltage falls below the 1.216 V threshold. When a voltage below 800mV is detected, the KEEP is set to low and UP is set high so that the counter increases the duty cycle. Simulation of this circuit is shown in Figure 8. The PWM output is shown in blue, and the input voltage is shown in yellow.

 Overvoltage and Undervoltage
                    PWM Circuit Figure 7 Overvoltage and Undervoltage PWM Circuit
 PWM Circuit Simulation Figure 8 PWM Circuit Simulation

As previously described in Counter FSM Functionality, the counter module counts down to 0 or up to 255 and then resets the count value. Thus, additional circuitry is required to pause cnt0 near the values of 0 or 255 to maintain the minimum and maximum duty cycle and prevent the counter from looping. This circuitry is shown in Figure 9; cntOV is configured with a control data of 125 (three lower than cnt0) and cntUV is configured with a control data of 131 (three higher than cnt0). Upon entering a overvoltage state, both cnt0 and cntOV are reset and begin counting down; cntOV counts to 0 before cnt0 due to having a lower control data, and the corresponding output pulse is latched by dff0 and used to set KEEP high and hold the current count value of cnt0. For an undervoltage state, cntUV operates the same way, counting up instead of down.

 PWM Looping Prevention Circuit Figure 9 PWM Looping Prevention Circuit

To maintain that cntOV and cntUV finish counting before cnt0, cnt0 must also be reset upon a transition to an overvoltage or undervoltage state. This means the duty cycle resets to 50% upon a transition to either state. The logic for controlling the reset and FSM signals into cnt0 is shown in Figure 10.

 PWM Counter FSM Control Circuit Figure 10 PWM Counter FSM Control Circuit

Additional Considerations

Figure 8 shows that the PWM output reaches the maximum and minimum duty cycle values rather quickly. More gradual changes in duty cycle can be achieved by setting the counter clocks slower than the PWM clock, although this can result in occasional glitching in the PWM output due to clock jitter and skew.

The PWM duty cycle can also be controlled using the I2C or SPI Receiver and writing the desired control data to the appropriate counter FSM's data register.

Conclusions

The PWM module allows for TPLD to generate square waves with varying duty cycles. By incorporating several different logic functions and analog sensors, TPLD provides an integrated design for real-time PWM generation and control.

Learn more about TI’s portfolio of programmable logic devices