SCPS309B August 2025 – June 2026 TXE8116
PRODUCTION DATA
In the event of a glitch or data corruption, TXE8116 can be reset to the default conditions by using the power-on reset feature. Power-on reset requires that the device go through a power cycle to be completely reset. This reset also happens when the device is powered on for the first time in an application.
The two types of power-on reset are shown in Figure 8-2 and Figure 8-3 .
Glitches in the power supply can also affect the power-on reset performance of this device. The glitch width (tVCC_GW) and height (VCC_GH) are dependent on each other. The bypass capacitance, source impedance, and device impedance are factors that affect power-on reset performance. Figure 8-4 provides more information on how to measure these specifications.
VPOR is critical to the power-on reset. VPOR is the voltage level at which the reset condition is released and all the registers and the SPI state machine are initialized to the default states. The value of VPOR differs based on the VCC being lowered to or from 0. Figure 8-5 provides more detail on this specification.