SDAA103 September 2025 IWRL6432AOP
To compute the Steering Vector Coefficient Matrix, TI measured the returned phase of the IWRL6432 over multiple PCB designs, units and temperatures. Using a Millibox miniature anechoic chamber and a corner reflector placed at a known distance from the radar, TI rotated the radar devices over a sweep of azimuth and elevation angles, and recorded the returned ADC data at each angle.
Figure 2-1 and Figure 2-2 show the setup that TI used with the radar on one end of the chamber and a corner reflector at the other end.
Figure 2-1 IWRL6432AOPEVM in Millibox
Chamber
Figure 2-2 Corner Reflector at the Opposite End
of Millibox Chamber