SDAA103 September   2025 IWRL6432AOP

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Angle of Arrival Estimation Theory: FFT Beamformer
    2. 1.2 Angle of Arrival Estimation Theory: Steering Vectors
  5. 2Additional Information
    1. 2.1 Measurement Procedure
    2. 2.2 Testing Results
      1. 2.2.1 Anechoic Chamber Testing on Corner Reflector Targets
      2. 2.2.2 Outdoor Testing on Human Subjects
    3. 2.3 Processing Time
    4. 2.4 Usage
    5. 2.5 Extensions to Other Platforms
  6. 3Summary
  7. 4References
  8. 5Appendix
    1. 5.1 Chirping Parameters for Each Configuration File
    2. 5.2 Point Cloud Data for Human Subject Testing

Angle of Arrival Estimation Theory: FFT Beamformer

Based off the theory in The Fundamentals of Millimeter Wave Radar Sensors, the angle of arrival of an object in the FOV in the radar can be estimated using Equation 1 and Equation 2.

Equation 1. ∆ Φ = 2 π ∆ d λ

If all the antennas are aligned in a planar wave-front, then basic geometry shows that Δd = lsin(θ)

Equation 2. θ = sin - 1 ⁡ λ ∆ Φ 2 π l

In practice, MIMO systems use more than two antennas though, so the change in phase (ΔΦ) is not just a change in phase across two antennas, but change in phase across N-antennas. Change in phase over space is known as spatial frequency (ω), and this can be estimated using an FFT.

Equation 3. θ = sin - 1 ⁡ λ ∆ Φ 2 π l = sin - 1 ⁡ λ ω 2 π l

The FFT is often padded with a large number of zeros to increase the number of candidate angles (seen on the X-axis). As a result, the angle FFT often produce broad peaks. Therefore, to estimate the angle-of-arrival of an object, the radar compares the magnitude of the FFT at all these different candidate locations, and select the peak (or peaks) that correspond to the maximum values in the angle-spectrum. The picture below illustrates this, and the selected peak is at index 11, since the magnitude is highest.

 Broad FFT Spectrum with Max Peak at
          Index 11 Figure 1-1 Broad FFT Spectrum with Max Peak at Index 11

On the IWRL6432, this FFT calculation is done using the radar hardware accelerator. However, this is fundamentally equivalent to a matrix-vector product of the FFT matrix with the received phase of all the antennas. The AOA that is selected is the angle which corresponds to the maximum value of ai in Equation 4.

Equation 4. w 0 w 0 ⋯ w 0 w 0 ω 1 ⋯ ω N - 1 ⋮ ⋯ ⋱ ⋮ w 0 ω N - 1 ⋯ ω N - 1 N - 1 ϕ 0 ϕ 1 … ϕ N - 1 = a 0 a 1 … a N - 1
Equation 5. ω = e - j 2 π N

From the vector of output correlation vector x, select the FFT index that corresponds to the maximum value of xi.

Equation 6. i d x e s t = a r g m a x i a i ⁡

Then, use the AOA formula to compute the estimated AOA θest.

Equation 7. i f i d x e s t ≤ N 2 → θ e s t = a s i n ⁡ 2 × i d x e s t N ⁡
Equation 8. i f i d x e s t > N 2 → θ e s t = a s i n ⁡ N - 2 × i d x e s t N ⁡