SDAA137 June 2026 UCD91160 , UCD91320
The black box fault logs in the UCD91xxx devices are designed to preserve the first and last faults that occur in the device. The first fault is written to the device non-volatile memory as soon as possible after it occurs, and the last fault is written when the device crosses the BOR voltage threshold. No additional configuration is required to enable the black box.