SDAA233 December 2025 TPS7H4102-SEP , TPS7H4104-SEP , TPS7H4104-SP
During operation, it is possible for VEXT to deviate from the nominal DC value due to external factors such as line transients, load transients (if VEXT is loaded), and single-event transients caused by radiation. The SEE report for the TPS7H4104-SEP, Single-Event Effects (SEE) Radiation Report of the TPS7H4104-SEP shows and discusses the results of testing the TPS7H4104-SEP under a heavy-ion beam. While no SET events 3% or greater in magnitude were observed, a theoretical 3% transient can be induced on VEXT in simulation to observe the effects on VOUT with different nominal levels of VEXT.
In the simulation, a -3% transient was injected directly onto the VEXT rail with rise and fall times of 10µs. Three different nominal VEXT levels were tested, and transient magnitude was adjusted for each VEXT condition to -3% of nominal. Figure 4-3 shows the results for all three VEXT levels displayed on a single plot.
The plot above shows that for larger values of VEXT, the same percentage deviation from the nominal voltage will produce a smaller disturbance on VOUT. The cause of this unintuitive relationship is the voltage drop across RB1, and the VREF voltage. The current flowing through RB1 is not determined by the total potential between GND and VEXT, but rather between VEXT and VREF. Since the magnitude of the upset on VEXT was determined by the VEXT to GND voltage, after VREF is subtracted from VEXT, smaller values of VEXT will end up with larger percentage upsets because VREF is a larger portion of the value.
In addition, a modified TPS7H4104EVM with VEXT and a low-voltage output channel in a similar configuration as described in section 3 and simulated in section 4 was exposed to a heavy ion beam with an LET of 75MeV. No SET events with a magnitude greater than 2.5% were observed on VOUT.