SDAA233 December   2025 TPS7H4102-SEP , TPS7H4104-SEP , TPS7H4104-SP

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Concept of Operation
  6. 3Maintaining Output Accuracy
  7. 4Simulation Results
    1. 4.1 VEXT Output Deviation Effects
  8. 5Test Results With TPS7H4104EVM
  9. 6Summary
  10. 7References

Test Results With TPS7H4104EVM

To verify this configuration outside of simulation, a TPS7H4104EVM evaluation module was modified to output 0.5V on CH3. Similarly to the previous simulation, the 1.2V output generated by CH2 was used as VEXT for the CH3 feedback divider. To implement this configuration, four modifications are required to the EVM which are circled in red in Figure 5-1.

  • R22 was replaced to set the device switching frequency to approximately 300kHz.
  • R17 was depopulated to remove the connection to GND of the feedback divider.
  • R33 was populated to be used as RB1
  • VEXT was connected to RB1.
 Modified EVM SchematicFigure 5-1 Modified EVM Schematic

The location of R17 is shown in Figure 5-2.

 Top-side EVM Board RenderFigure 5-2 Top-side EVM Board Render

Modifications to the bottom of the EVM are shown in Figure 5-3. When R33 (RB1) is populated, one pad is connected through a via to VSNS3, while the other pad is connected to a trace that leads to R41. Since R41 is not populated, the left-side pad of R41 can be connected through an external wire to VOUT2 (VEXT), this was done by connecting to the bottom side of the VOUT2 test point. The trace connecting R33 to R41 now provides VEXT to RB1, completing the modified feedback circuit.

 Bottom-Side EVM Board RenderFigure 5-3 Bottom-Side EVM Board Render

The modified EVM was powered on with the internal sequencer enabled, and the startup was recorded with a 3A load on VOUT.

 EVM Startup ResultFigure 5-4 EVM Startup Result

As expected, the output from the modified EVM matches closely with the simulation results in Figure 4-2, providing a 0.5V output on CH3 using the 1.2V VEXT generated from CH2.