SDAA233 December   2025 TPS7H4102-SEP , TPS7H4104-SEP , TPS7H4104-SP

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Concept of Operation
  6. 3Maintaining Output Accuracy
  7. 4Simulation Results
    1. 4.1 VEXT Output Deviation Effects
  8. 5Test Results With TPS7H4104EVM
  9. 6Summary
  10. 7References

Concept of Operation

Methods to lower a converter's output voltage below the reference are explored in the application notes SLVA216 and SLUAAO0. When these methods are implemented in a feedback divider of the regulator, an external voltage source (VEXT) is connected to the feedback node through a resistor (REXT). By varying the voltage of VEXT and the values of the feedback resistors, the voltage at the output of the regulator can be set. With set feedback resistor values, when VEXT is raised, VOUT drops, and when VEXT is lowered, VOUT rises.

 Three Resistor Simplified SchematicFigure 2-1 Three Resistor Simplified Schematic

When VEXT is greater than VREF, current from VEXT flows to GND through REXT and RB1. The additional current from VEXT though RB1 causes a voltage rise at VSNS. The control loop of the regulator senses this voltage rise and decreases VOUT in response, causing current flow through RB1 from RT1 to decrease. As the current through RB1 decreases, the voltage at VSNS decreases and returns to the reference voltage, but now with VOUT at a lower level. If enough current is allowed to flow through RB1 such that the current through the top feedback resistor goes to zero, VOUT is equal to the reference voltage of the regulator. If the current through REXT is increased beyond this point, then VOUT drops below the reference voltage. During this condition, current no longer flows from VOUT to GND through the feedback divider but rather flows from VEXT to VOUT and to GND through RT1 and RB1.

 Simplified Schematic With Current FlowFigure 2-2 Simplified Schematic With Current Flow

In this operating mode RB1 is no longer required, as this mode no longer contributes to the feedback functionally and only serves as a source of error. The bottom resistor can then be removed and replaced with REXT which then becomes the new RB1 in the divider.

 Two Resistor Simplified SchematicFigure 2-3 Two Resistor Simplified Schematic

In this new configuration, the feedback resistor divider is now formed between VEXT, and VOUT. When the voltage of VEXT is greater than VREF, to maintain VSNS at the reference voltage, VOUT must be lower than VREF to accommodate the voltage drop across R­T1. Stable regulation is still maintained, as when VOUT drops or rises, the voltage at VSNS still drops or rises proportionally, as with a standard implementation. VOUT in this configuration is now determined by the values of RT1, RB1, VREF, and VEXT.

Equation 1. VOUT=RT1×VREF-VEXTRB1+VREF

The configuration shown in Figure 2-3 is already useful, as it allows for VOUT to be regulated below the reference with only the addition of an external voltage source. However, the problem it introduces can be seen in the equation for VOUT. Since the output voltage is dependent on both VREF and VEXT, errors in both terms must now be considered when calculating output accuracy of the regulator. Since VEXT is not an accurate voltage source, in this configuration the accuracy of the regulator is permanently degraded by the accuracy of whatever external voltage source is used for VEXT.