SDAA249 January   2026 AMC3330-Q1 , INA148-Q1 , TPS61170-Q1 , TPSI2240-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Background
    2. 1.2 Operation Principle
  5. 2Hardware Design
    1. 2.1 Solid State Relay (SSR)
    2. 2.2 Resistors
      1. 2.2.1 Minimum Resistance
      2. 2.2.2 Maximum Resistance
      3. 2.2.3 Resistance Ratio
    3. 2.3 Bias Supply
    4. 2.4 Amplifier
      1. 2.4.1 MCU on the Low Voltage Side
      2. 2.4.2 MCU on the AC Side
  6. 3Software Design
    1. 3.1 Settling Time
    2. 3.2 SSR Sequence
    3. 3.3 Voltage Threshold
    4. 3.4 Moving Average
    5. 3.5 Plausibility Check
    6. 3.6 Control Scheme Summary
  7. 4Simulation Results
    1. 4.1 Settling Time
    2. 4.2 Input Voltage Range
    3. 4.3 Plausibility Check
    4. 4.4 Accuracy
    5. 4.5 Influence of the Y Capacitor
  8. 5Summary
  9. 6References

Accuracy

The accuracy of the IMD is related to many factors, such as the precision of resistors, the value of Y capacitors, the deviation of the DC bias supply, the error on the amplifier, and the settling time. The most reliable way to assess the accuracy of the IMD is through hardware testing. The simulation is only used to verify whether insulation failures can be detected under several typical operating conditions.

For the case of an asymmetric insulation failure, as can be seen from Table 4-2, when the insulation resistance drops below 90kΩ, VIN_AVG exceeds the 1.8V threshold, and the insulation failure is detected. When the insulation resistance is greater than 200kΩ, even if VIN_AVG exceeds 1.8V due to various errors, the peak value of VIN is still below the 2.5V threshold, which means a plausibility check prevents false reporting of an insulation failure.

For the case of a symmetric insulation failure, the VIN peak voltage and VIN_AVG can be found in Table 4-3. When the insulation resistance drops below 90kΩ, VIN_AVG exceeds the 1.8V threshold, and the insulation failure is detected. When the insulation resistance is greater than 500kΩ, the VIN_AVG is 60mV lower than the 1.8V threshold, so an insulation failure is not falsely triggered.

Table 4-3 Sensed Voltage in Different Insulation Resistance
RisoL RisoN VIN Peak VIN_AVG Plausibility Check Applicable Insulation Failure
10MΩ 10MΩ 1.51V 1.51V No No
1MΩ 1MΩ 1.69V 1.69V No No
500kΩ 500kΩ 1.74V 1.74V No No
200kΩ 200kΩ 1.79V 1.79V No No
90kΩ 90kΩ 1.81V 1.81V No Yes
0kΩ 0kΩ 1.83V 1.83V No Yes

The trickiest situation occurs when a symmetric insulation failure happens, and the insulation resistances are both around 200kΩ. This is because 1.79V VIN_AVG is very close to the 1.8V threshold, so making an insulation failure falsely trigger can easily occur.

A false trigger at 200kΩ is not so bad, since the insulation resistance is expected to be megaohms and the threshold is 110kΩ, so if the insulation is 200kΩ there is already something wrong in the system. As mentioned in Section 3.5, for this kind of scenario, the proposal is to sample a longer time and take the average to minimize the impact of dynamic errors on sampling accuracy.