SDAA437 July 2026 TDA4VE-Q1
After identifying the OSPI MTD partitions, the boot components can be flashed into OSPI NOR flash.
During development, the boot component images were obtained from the SD card boot partition used to boot the J721S2 EVM. The locations of the boot component images will be found at /run/media/BOOT-mmcblk1p1 as follows.
root@j721s2-evm:~# ls -l /run/media/BOOT-mmcblk1p1/
total 4906
-rwxrwx--- 1 root disk 465805 Jun 13 2026 tiboot3-j721s2-gp-evm-j721s2-evm-k3r5-2025.01+git97201+743712b-r0_tisdk_6_edgeai_5.bin
-rwxrwx--- 1 root disk 465805 Jun 13 2026 tiboot3-j721s2-gp-evm.bin
-rwxrwx--- 1 root disk 468394 Jun 13 2026 tiboot3-j721s2-hs-evm.bin
-rwxrwx--- 1 root disk 468394 Jun 13 2026 tiboot3-j721s2-hs-fs-evm.bin
-rwxrwx--- 1 root disk 465805 Jun 13 2026 tiboot3.bin
-rwxrwx--- 1 root disk 1326915 Jun 13 2026 tispl.bin
-rwxrwx--- 1 root disk 1359931 Jun 13 2026 u-boot.img
-rwxrwx--- 1 root disk 941 Jun 13 2026 uEnv.txt
-rwxrwx--- 1 root disk 14 Jun 13 2026 version
Table 4-1 shows the mapping between the boot component images and their target OSPI partitions.
| Image | Target MTD Device | OSPI Partition |
|---|---|---|
| tiboot3.bin | /dev/mtd0 | ospi.tiboot3 |
| tispl.bin | /dev/mtd1 | ospi.tispl |
| u-boot.img | /dev/mtd2 | ospi.u-boot |
The boot components are flashed using the Linux flashcp utility.
root@j721s2-evm:~# flashcp /run/media/BOOT-mmcblk1p1/tiboot3.bin /dev/mtd0
root@j721s2-evm:~# flashcp /run/media/BOOT-mmcblk1p1/tispl.bin /dev/mtd1
root@j721s2-evm:~# flashcp /run/media/BOOT-mmcblk1p1/u-boot.img /dev/mtd2
After flashing completes, the OSPI NOR flash contains all boot software required to reach the U-Boot prompt. The next section verifies that the flashed images can be successfully loaded when the board is configured for OSPI boot mode.