SDAA437 July 2026 TDA4VE-Q1
Create the minimal directory structure required by the root filesystem.
mkdir -p /mnt/ospi_rootfs/bin
mkdir -p /mnt/ospi_rootfs/usr/lib
mkdir -p /mnt/ospi_rootfs/dev
mkdir -p /mnt/ospi_rootfs/proc
mkdir -p /mnt/ospi_rootfs/sysCopy BusyBox into the root filesystem.
cp /usr/bin/busybox /mnt/ospi_rootfs/bin/Copy the required shared libraries.
cp /usr/lib/libm.so.6 /mnt/ospi_rootfs/usr/lib/
cp /usr/lib/libc.so.6 /mnt/ospi_rootfs/usr/lib/
cp /usr/lib/ld-linux-aarch64.so.1 /mnt/ospi_rootfs/usr/lib/These libraries can be identified using ldd command.
ldd /usr/bin/busyboxThis application note uses a BusyBox-based minimal root filesystem to reduce complexity and focus on the essential Linux boot process.