SDAA443 August   2026 CC3300 , CC3300MOD , CC3301 , CC3301MOD , CC3350 , CC3350MOD , CC3351 , CC3351MOD , CC3501E , CC3551E

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1 Required Items
  5. 2 Overview of Available Tools
  6. 3 Getting Started with Radio Tool
  7. 4 Getting Started with Calibrator Tool
  8. 5 Wi-Fi Testing
    1. 5.1 TX Testing Using Radio Tool
      1. 5.1.1 802.11ax Trigger Based Testing
    2. 5.2 TX Testing Using Calibrator Tool
      1. 5.2.1 802.11ax Trigger Based Testing
    3. 5.3 RX Testing Using Radio Tool
    4. 5.4 RX Testing Using Calibrator Tool
  9. 6 BLE Testing
    1. 6.1 TX Power Using Radio Tool
    2. 6.2 TX Power Using HCI Commands
    3. 6.3 RX Sensitivity Using Radio Tool
    4. 6.4 RX Sensitivity Using HCI Commands
  10. 7 Troubleshooting/FAQs
  11. 8 Duty Cycle Table
  12. 9 Summary
  13. 10References

TX Testing Using Calibrator Tool

If Calibrator tool has not been set up, navigate to the Getting Started with Calibrator Tool section before continuing. Use the below example flows as references for how to perform a TX test. For further information on Calibrator Tool, navigate to the Calibrator Tool guides for the CC33xx and CC35xx located in the respective SDKs.

CC33xx example flow on channel 6, with 11ax SU preamble type, MCS6 rate, TX power 21:

calibrator wlan0 plt power_mode on 
calibrator wlan0 cc33xx_plt tune_channel 6 0 0 
calibrator wlan0 cc33xx_plt set_manual_calib -tx 1
calibrator wlan0 cc33xx_plt set_tx -preamble_type 5 -phy_rate 19 -tx_power 31
calibrator wlan0 cc33xx_plt start_tx
calibrator wlan0 cc33xx_plt stop_tx

CC35xx example flow on channel 6, with 11ax SU preamble type, MCS6 rate, TX power 21:

wlan_start
calibrator power_mode on 
calibrator tune_channel 6 0 0 
calibrator set_manual_calib -tx 1
calibrator set_tx -preamble_type 5 -phy_rate 19 -tx_power 31
calibrator start_tx
calibrator stop_tx

Note: Figure 5-4 provides assistance when tuning the device. The parameters should be typed in the order they appear.


 TX Parameters Table

Figure 5-4 TX Parameters Table

On the VSA, configure the tables so that TX Power, EVM and Frequency Error can be viewed. Varying the TX Power, Preamble Type and Phy Rate must confirm the device meets datasheet TX Power specifications as well as the 802.11 EVM and Frequency Accuracy standards.