SDAA443 August   2026 CC3300 , CC3300MOD , CC3301 , CC3301MOD , CC3350 , CC3350MOD , CC3351 , CC3351MOD , CC3501E , CC3551E

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1 Required Items
  5. 2 Overview of Available Tools
  6. 3 Getting Started with Radio Tool
  7. 4 Getting Started with Calibrator Tool
  8. 5 Wi-Fi Testing
    1. 5.1 TX Testing Using Radio Tool
      1. 5.1.1 802.11ax Trigger Based Testing
    2. 5.2 TX Testing Using Calibrator Tool
      1. 5.2.1 802.11ax Trigger Based Testing
    3. 5.3 RX Testing Using Radio Tool
    4. 5.4 RX Testing Using Calibrator Tool
  9. 6 BLE Testing
    1. 6.1 TX Power Using Radio Tool
    2. 6.2 TX Power Using HCI Commands
    3. 6.3 RX Sensitivity Using Radio Tool
    4. 6.4 RX Sensitivity Using HCI Commands
  10. 7 Troubleshooting/FAQs
  11. 8 Duty Cycle Table
  12. 9 Summary
  13. 10References

TX Power Using Radio Tool

Select BLE TX in the left column. The screen should match Figure 6-1. If not, or if Radio Tool has not yet been set up, navigate to the Getting Started with Radio Tool section first and follow the steps.


 BLE TX Homepage in Radio
                    Tool

Figure 6-1 BLE TX Homepage in Radio Tool
  1. Configure the settings as desired such as BLE Channel, RF Mode, TX Power, and so on.
  2. For a smoother testing experience, turn the Infinite Packet Transmit toggle on. With this toggle off, the user has to repeatedly click Calibrate and TX Start every time they want to send more packets, which is tedious.
  3. Click Calibrate. TI recommends doing this before every TX Start.
  4. Before starting transmission, make sure to configure the VSA properly. If using LitePoint, your screen should resemble Figure 6-2

     Example LitePoint
                            Screen Configuration

    Figure 6-2 Example LitePoint Screen Configuration
  5. Run Continuous Analysis on the VSA. In Radio Tool, click TX Start.
Note: Always account for loss in the setup. As seen in the images above, there is a 3 dBm discrepancy due to cable loss. If measured TX Power is still below the value set in Radio Tool, refer to the Troubleshooting/FAQ section.