SDAA443 August 2026 CC3300 , CC3300MOD , CC3301 , CC3301MOD , CC3350 , CC3350MOD , CC3351 , CC3351MOD , CC3501E , CC3551E
My device is failing to calibrate when using a TI EVK:
I'm seeing lots of error packets when my device is in RX mode: Depending on the testing setup, you may have a capacitor that either runs from the RF connector to the chip, or the antenna to the chip. For conductive testing, if the capacitor faces the antenna rather than the RF connector, packets may be misinterpreted. The same issue can occur in over-the-air testing if the capacitor faces the RF connector.
My VSA is not picking up any data or my device is not receiving any packets: Verify that the test instrument port mode matches the test type: TX tests require the instrument to be in VSA mode; RX tests require it to be in VSG mode. Additionally, verify that the DUT and the testing instrument are on the same channel.
I am performing 802.11ax Trigger Based (TB) testing but my VSA is not reading any data: Trigger based testing involves several more settings, regardless of using Radio Tool or Calibrator Tool, and these must be matched exactly on the VSA. These settings include: GI LTF type, Number of LTF, RU Allocation and PHY rate.
I am seeing a lower TX Power value than expected: