SDAA510 October 2026 AM2431 , AM2432 , AM2434 , AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
If the USB driver is working properly and the J-Link / J-Trace is connected with the host system, the user can connect J-Link / J-Trace to the target hardware. Start J-Link Commander (JLink.exe) which must now display the normal J-Link / J-Trace related information, such as the hardware version and firmware version. After issuing the connect command and providing the additional information required to connect to the device, the J-Link connects to the device. Additional information about the target is shown (for example. ROM-Table).
Follow the steps:
Figure 4-1 Connect Command
Figure 4-2 Device and Core SelectionMore details on SEGGER J-Link Commander can be found at https://kb.segger.com/J-Link_Commander