SDAA510 October 2026 AM2431 , AM2432 , AM2434 , AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
To Flash the AM243x/AM64x EVM, use J-Flash. J-Flash is a stand-alone flash programming software for PCs running Windows, Linux or macOS.
J-Flash has an intuitive user interface and makes programming flash devices convenient. J-Flash requires a J-Link / Flasher as an interface to the target hardware.
Below are the steps to flash the hello world example using J-Flash.
Steps to Flash using J-Flash:
Figure 5-1 DEV
Boothalt // Halt R5FSS0_CORE0
//
// !!! TODO: Update TI AM243x/AM64x SDK path !!!
//
loadfile "C:\TI\mcu_plus_sdk_{device}_{version}\tools\ccs_load\\{device}\sciclient_ccs_init.release.out"
setpc 0x0 // Set program counter to start of RAM
go // Start R5FSS0_CORE0
exit // Close J-Link Commander
Figure 5-2 J-Flash ConfigAfter successful execution of above steps, the binaries are now flashed. Change the boot mode to OSPI and the user can see the OSPI SBL and Hello world logs onto the UART console after the EVM is turned on.
Figure 5-3 OSPI BootAfter successfully flashing an image which contains an SBL, successive flash programming operations can be executed in SPI Boot Mode without requiring the initialization steps one through three and the steps in the codeblock. See the following documentation from SEGGER J-Link for Flashing purpose.