SDAA515 August 2026 TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The reference implementation was evaluated using a 4GB DDR configuration.
| DDR Capacity | Priming Time |
|---|---|
| 4GB | Approximately 147ms |
The result demonstrates that DRU-based initialization can efficiently generate ECC information across the entire protected DDR address space while maintaining acceptable start-up overhead.
Actual priming time can vary depending on:
Figure 2-4 illustrates the ECC error reporting path.
Correctable errors (CE) are automatically corrected by the DDR subsystem, while uncorrectable errors (UE) are reported through the ESM for software handling.