SDAA561 October 2026 AFE58JD18 , AFE58JD28 , AFE58JD48 , THS4551 , THS4567
Based on the brief introduction above, we have gained a basic understanding of differential amplifiers. Just as with operational amplifiers, the effect of feedback verifies that the voltage at the non-inverting input of a fully differential amplifier equals the voltage at the inverting input. This principle can be used to determine the relationship between the circuit's output and input. Furthermore, in practical designs, the two feedback resistors in a fully differential amplifier are typically chosen to have equal values to simplify calculations.