SDAA569 October   2026 ISO6020 , ISO6021 , ISO6040 , ISO6041 , ISO6042 , ISO6061 , ISO6062 , ISO6063 , ISO6420 , ISO6420-Q1 , ISO6421 , ISO6421-Q1 , ISO6431 , ISO6440 , ISO6440-Q1 , ISO6441 , ISO6441-Q1 , ISO6442 , ISO6442-Q1 , ISO6461 , ISO6462 , ISO6463 , ISOW6441

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2How to Determine if a Digital Isolator Has Overvoltage-Tolerant Inputs?
  6. 3The Benefits of Digital Isolators with Overvoltage-Tolerant Inputs
    1. 3.1 Accept Higher-Than-Supply Input Levels Safely
    2. 3.2 Simplify Interfacing Between Devices with Different Supplies or Power Sequences
    3. 3.3 Improve Robustness During Brown-Out Conditions
    4. 3.4 Reduce Power Consumption by Powering Down During Normal System Operation
    5. 3.5 Withstands Signal Overshoots Due to Parasitics
    6. 3.6 Preserve Signal Integrity by Avoiding Extra Filtering Networks During EMC Transients
    7. 3.7 Reduce Board Area Utilization
  7. 4Digital Isolators with Overvoltage Tolerant Inputs
  8. 5Summary
  9. 6References

How to Determine if a Digital Isolator Has Overvoltage-Tolerant Inputs?

Digital isolators that feature overvoltage-tolerant inputs can accommodate voltages exceeding the device’s supply voltage. Verify this capability by checking the datasheet’s absolute maximum ratings section where the input voltage specification indicates if the inputs are overvoltage tolerant.

In the datasheets of digital isolators, such as the ISO6741, find the input voltage rating specified as VCC + 0.5V (Figure 2-1). This indicates that the permissible input voltage is tied directly to the VCC supply voltage. Exceeding this limit violates the absolute maximum ratings specification and can damage the device, therefore, these devices do not support overvoltage tolerant inputs.

 Absolute Maximum Ratings of a Digital
          Isolator Without Overvoltage-Tolerant Inputs Figure 2-1 Absolute Maximum Ratings of a Digital Isolator Without Overvoltage-Tolerant Inputs

In the datasheets of digital isolators that feature overvoltage-tolerant inputs, the allowable input voltage is often specified as a fixed range — for example, –0.5V to 6V (Figure 2-2). Unlike the ISO6741, where the input limit is expressed relative to VCC, this voltage range is independent of the supply voltage. Therefore, the signal can be applied to the input even when the supply is powered down, provided it remains within the absolute maximum ratings limits.

 Absolute Maximum Ratings of a Digital
          Isolator with Overvoltage-Tolerant Inputs Figure 2-2 Absolute Maximum Ratings of a Digital Isolator with Overvoltage-Tolerant Inputs