SDAA601 November   2026 AM13E23019

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Prerequisites
  6. 3How to Setup and Use the Tool
  7. 4Getting Started Fast: AI as a Bootstrap for New Projects
    1. 4.1 Identify the Target Device and Connected Hardware
    2. 4.2 Use SDK and Device-Specific Guidance
    3. 4.3 Start with Import a Matching Example Project
    4. 4.4 Configure Peripherals through SysConfig Using Natural Language
    5. 4.5 Write the Functionally Validated Application Code
    6. 4.6 Build and (If Starter Kit is Present) Flash and Run
  8. 5Debugging Through the Probe: AI-Driven Control Over Real Hardware
  9. 6Migrating Projects from Other MCU Ecosystems
  10. 7Supported Devices and Peripherals
  11. 8Summary
  12. 9References

Summary

This document discusses a few use cases on how to use the ASM AI assistant migration tool for developing a new project from the beginning as well as migrating the example from older platforms. While there are other use cases such as prompting AI to learn about device architecture and to understand peripherals, these use cases are up to the the user to execute.