SDAA601 November   2026 AM13E23019

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Prerequisites
  6. 3How to Setup and Use the Tool
  7. 4Getting Started Fast: AI as a Bootstrap for New Projects
    1. 4.1 Identify the Target Device and Connected Hardware
    2. 4.2 Use SDK and Device-Specific Guidance
    3. 4.3 Start with Import a Matching Example Project
    4. 4.4 Configure Peripherals through SysConfig Using Natural Language
    5. 4.5 Write the Functionally Validated Application Code
    6. 4.6 Build and (If Starter Kit is Present) Flash and Run
  8. 5Debugging Through the Probe: AI-Driven Control Over Real Hardware
  9. 6Migrating Projects from Other MCU Ecosystems
  10. 7Supported Devices and Peripherals
  11. 8Summary
  12. 9References

Start with Import a Matching Example Project

Instead of generating a new project structure, the tool uses the SDK project as a starting point. The advantages are SDK-validated examples, the build system, linker command file, and startup code that are already correct, making sure there are minimal build hiccups.