SDAA601 November   2026 AM13E23019

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Prerequisites
  6. 3How to Setup and Use the Tool
  7. 4Getting Started Fast: AI as a Bootstrap for New Projects
    1. 4.1 Identify the Target Device and Connected Hardware
    2. 4.2 Use SDK and Device-Specific Guidance
    3. 4.3 Start with Import a Matching Example Project
    4. 4.4 Configure Peripherals through SysConfig Using Natural Language
    5. 4.5 Write the Functionally Validated Application Code
    6. 4.6 Build and (If Starter Kit is Present) Flash and Run
  8. 5Debugging Through the Probe: AI-Driven Control Over Real Hardware
  9. 6Migrating Projects from Other MCU Ecosystems
  10. 7Supported Devices and Peripherals
  11. 8Summary
  12. 9References

Getting Started Fast: AI as a Bootstrap for New Projects

This section talks about how this tool can be used for an accelerated getting started experience. In a traditional setup, a developer who wants to prototype an idea: blink an LED, stream ADC samples over UART, drive a motor with a PWM pattern — has to context-switch between a device datasheet, a reference manual, SDK example code, and the IDE itself before starting actual prototyping.

With the AM13x AI Assisted Development and Migration tool built into the CCStudio IDE, the bootstrapping process collapses into a conversation. The goal can be described in plain language (the peripheral configuration and required setup) and the AI model: