SLAAE25 May 2021 MSP430FR2355 , MSP430FR2355
There is a GUI for this solution that can help you quickly evaluate and adjust parameters. The GUI communicate with MCU through UART, MCU can send the collected real-time ADC data to PC. And You can check if the parameter in the code are reasonable by observing the current ADC value.
Figure 6-1 GUI for Pulse OximeterConnect the Demo board and GUI through the following steps:
Figure 6-2 shows the data sent by the MCU to the GUI.
Figure 6-2 Data in GUI for Pulse
Oximeter