SLAAEI7 December 2023 MSPM0C1105 , MSPM0C1106 , MSPM0G1106 , MSPM0G1107 , MSPM0G1506 , MSPM0G1507 , MSPM0G1518 , MSPM0G1519 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3518 , MSPM0G3518-Q1 , MSPM0G3519 , MSPM0G3519-Q1 , MSPM0H3215 , MSPM0H3216
The internal OPA of the MSPM0 has a chopping feature which reduces the drift of the OPA. This chopping is configurable to adapt to different use cases and signal chains. The chopping must be adjusted to the ADC-assisted chopping mode when using the ADC in oversampling and averaging mode. This adjustment prevents the chopping frequency from interfering with the averaging feature of the ADC. Figure 4-1 is a resulting histogram showing two maxima in the distribution of a series of values where the standard chopping mode is used with ADC averaging. Figure 4-1 demonstrates that the effective resolution of the signal chain is significantly reduced.