SLAAEL7A June   2024  – November 2026 TAS2572

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Voltage Limiter Based Battery Guard
  6. 3Advanced Battery Guard
    1. 3.1 Tracking of ESR
    2. 3.2 Speaker Load Tracking
    3. 3.3 Effect of Decoupling Capacitor
  7. 4Summary
  8. 5References
  9. 6Revision History

Introduction

Battery-operated systems (like mobile phones) required a boosted audio amplifier to be able to drive high peak voltage (power) into the speaker. In such systems, the battery voltage sees a ripple whose amplitude depends upon:

  • Battery internal resistance
  • External parasitic resistance
  • Decoupling capacitance

The combination of the battery internal resistance and external parasitic resistance is represented as External Series Resistance (ESR) of the system.

When the current drawn is too high, the drop in battery voltage increases to an extent that can cause clipping of the audio. The clipping can also result in the battery voltage dropping below the brownout threshold. Figure 1-1 shows a typical battery-powered audio system, and Figure 1-2 shows the corresponding drop seen in the battery voltage due to high current.

When the current drawn is too less, there is no clipping in the audio, however there can be higher headroom between the available, where the device can be capable of driving higher power into the speaker that what is being driven.

Thus, the requirement is to regulate the current drawn from the battery to maximize the loudness of the audio while preventing clipping at the same time.

 Representation of a
                        Battery-Powered Audio AmplifierFigure 1-1 Representation of a Battery-Powered Audio Amplifier
 VBAT Profile During Audio
                        PlaybackFigure 1-2 VBAT Profile During Audio Playback