SLAAEU0 April 2025 MSPM0C1105 , MSPM0C1105 , MSPM0C1106 , MSPM0C1106 , MSPM0H3216 , MSPM0H3216 , MSPM0L1306 , MSPM0L1306
Figure 2-1 shows the system block diagram. In the setup, use a power supply, a Li-ion battery, a MSPM0L1306 LaunchPadâ„¢ and a BQ2562x EVM. Users can do the setup by following the instructions.
Figure 2-1 System Block DiagramA real setup picture is shown in Figure 2-2.
Figure 2-2 Real Hardware SetupFor MSPM0L1306 LaunchPad, PA1 is configured as SCL pin, and PA0 is configured as SDA pin. The MSPM0L1306 is powered using the USB port on the host computer. Table 2-1 shows the signal and power connections between the two EVMs.
| Connection Type | Connection Name |
LP-MSPM0L1306 Pin Number |
BQ2562xEVM Pin Number |
|---|---|---|---|
| I2C interface | I2C : SCL | PA1 | J7-3 |
| I2C : SDA | PA0 | J7-2 | |
| Power connections | Power : Ground | J1-1 | J7-1 |
For the I2C interface, besides the connection of SCL and SDA, there are pull-up designs on both boards. The default hardware setting works well. Users can also select one EVM to pull up the SDA and SCL based on the application.
For the BQ2562x EVM, shorting JP2 and JP3 can pull up the SDA and SCL. The default value of the pull-up resistor is 10k ohm. This needs to be adjusted according the I2C bus speed. Figure 2-3 shows the pull-up jumper diagram on the BQ2562x EVM.
Figure 2-3 Pull-up in EVMFor the LaunchPad, shorting J9-2-3 and J10-2-3 can pull up the SDA and SCL. The default value of the pull-up resistor is 2.2k ohm. This can also be adjusted according the I2C bus speed. Figure 2-4 shows the pull-up jumper diagram on MSPM0L1306 LaunchPad.
Figure 2-4 Pull-up in LaunchPad