SLAAEU5A June 2025 – September 2025 TAS2780 , TAS2781
The TAS2781 and TAS2783 devices are highly configurable and support multiple power supply configurations to accommodate various system requirements. The devices can operate using both PVDDL and PVDDH supply rails for dynamic switching through the Y-Bridge architecture, or the devices can be configured to run exclusively from either PVDDH or PVDDL.
Table 3-1 summarizes the available power supply modes and the corresponding use cases, enabling designers to select the most efficient configuration based on application-specific needs.
| Power Modes | PVDDL_MODE | CDS_MODE | Y-Bridge | Description |
|---|---|---|---|---|
| PWR_MODE0 | 0 | 10 | Disabled | Both PVDDH and PVDDL are externally supplied to the device; however, only PVDDH is utilized for Class-D switching, while PVDDL powers the gate drivers and internal circuitry. |
|
PWR_MODE1 (default) |
0 | 00 | Enabled | Both PVDDH and PVDDL are supplied to the device externally and used for Class D switching. The Y-Bridge feature is enabled in this mode. |
| PWR_MODE2 | 1 | 11 | Enabled | Only PVDDH is supplied externally, while PVDDL is generated internally by the device. Both PVDDH and PVDDL are used for Class-D switching, and the Y-Bridge feature is enabled. When the audio signal level exceeds the default threshold of –71.5 dBFS, as defined by the LVS_TH_LOW[2:1], the Class-D output switches to the PVDDH. Only the idle channel switching occurs from PVDDL. |
| PWR_MODE3 | 0 | 01 | Disabled | Only PVDDL is supplied to the device externally, and the device can be forced to operate solely from the PVDDL rail for Class-D switching. However, the PVDDH supply is still required and must satisfy the condition PVDDH > PVDDL + 0.7V to make sure of proper device operation, even though PVDDH is not actively used for audio switching in this mode. |
| Address | Field [Bits] | Type | Reset | Description |
|---|---|---|---|---|
| 0x04 | PVDDL_MODE[7] | RW | 21h | PVDDL supply is 0h = Supplied externally (default) 1h = Internally generated from PVDDH |
| 0x03 | CDS_MODE[7:6] | RW | 28h | Class-D switching mode 0h = PWR_MODE1 (default) 1h = PWR_MODE3 2h = PWR_MODE0 3h = PWR_MODE2 |
This application note focuses specifically on PWR_MODE1 and PWR_MODE2, as these are the two configurations that support the Y-Bridge feature as shown in Table 3-1 and is discussed in detail in the following sections.