SLASEJ4C April 2017 – February 2023 PGA460
PRODUCTION DATA
The device wakes up immediately after a deglitched falling edge on the IO pin is detected. The controller must generate a wake-up signal defined as a dominant pulse (logic 0) on the time command interface with a length of at least 300 µs. After the wake-up pulse is complete, at least one command processing dead-time must be allowed before starting a time-command pulse which is shown in #X5729.
Figure 7-35 Time Command Interface Wake-Up Pulse