SLAU358Q September 2011 – October 2019
MSPGANG_CreateGangImage creates a command script and the data to be written to target devices according to current MSP-GANG configuration. After the image data is prepared, then it can be saved in the selected image memory by calling the MSPGANG_LoadImageBlock function.
Syntax
LONG MSPGANG_CreateGangImage(LPTSTR name)
Arguments
| LPTSTR name | Image name; maximum of 16 characters. Image name is displayed on the LCD display. |
Result
| LONG | Error code |