SLAZ769 December 2025 MSPM33C321A
SYSPLL Module
Functional
SYSPLL Frequency may not lock to correct frequency when enabled.
When setting the SYSPLLEN bit to 1 in SYSCTL HSCLKEN register, the SYSPLL will run the phase locked loop search. The search can potentially fail where the frequency will not be set to the correct value, instead the resultant frequency will be drastically different than the configured frequency.
Check the frequency output of the SYSPLL using the Frequency Clock Counter (FCC) anytime the SYSPLLEN bit is set to 1. Once the frequency is correct it will maintain the correct value until disabled and reenabled (SYSPLLEN set to 0 then 1), once reenabled the PLL will re-run the search and the SYSPLL output will need to be rechecked.
Workaround 1: Set FCC with SYSPLLCLK0 as the CLK input and LFCLK as the Trigger source. Run the FCC and check the value for the configured SYSPLL frequency with reference to the LFCLK; for example, with SYSPLL = 80MHz and LFCLK = 32kHz, the resultant FCC count should be 80,000,000/32,768= ~2441. The count will vary depending on the combined clock accuracies, so it is recommended to add a +-5% to allowed range. Estimated time for FCC is 30us.
FCC Settings: SYSCTL.GENCLKCFG.FCCTRIGCNT = 0, SYSCTL.GENCLKCFG.FCCTRIGSRC = 1, SYSCTL.GENCLKCFG.FCCSELCLK = 4;
If the FCC value is incorrect, disable and reenable the SYSPLL by setting SYSPLLEN to 0 then 1. Rerun the FCC check.
Workaround 2: Output SYSOSC/2 from the CLK_OUT pin and route the signal into FCC_IN. Use the SYSPLLCLK0 as the FCC CLK and the FCC_IN for the trigger source. Run the FCC for 16 Clock cycles, and check the value for the configured SYSPLL frequency with reference to the SYSOSC; for example, with SYSPLL = 80MHz and SYSOSC/2 = 16MHz, the resultant FCC count should be 80,000,000/16,000,000 * 16 = ~80. The count will vary depending on the combined clock accuracies, so it is recommended to add a +-5% to allowed range. Estimated time for FCC is 1us.
FCC Settings: SYSCTL.GENCLKCFG.FCCTRIGCNT = 0x0F, SYSCTL.GENCLKCFG.FCCTRIGSRC = 0, SYSCTL.GENCLKCFG.FCCSELCLK = 4;
If the FCC value is incorrect, disable and reenable the SYSPLL by setting SYSPLLEN to 0 then 1. Rerun the FCC check.