SLAZ769 December 2025 MSPM33C321A
GPIO Module
Functional
Writing to GPIO DOUTTGL registers might get missed when a DMA transfer is ongoing
The GPIO DMAMASK register information is mistakenly applied to a CPU write to the DOUTTGL register when a concurrent DMA transfer is in progress.
In the application code, ensure that the GPIO DMAMASK bit is set to 1 for the corresponding bit in the DOUTTGL register, before a CPU write access to the DOUTTGL register is issued. If no DMA transfer to any of the GPIO registers is required, the GPIO DMAMASK can be configured as 0xFFFFFFFF during the IO initialization step. This will solve the conflict of this errata. If the application also requires DMA write transfers to the GPIO registers, it is recommended that the application not use both DMA and CPU to write to the DOUTTGL register of the same GPIO module in the device. If the device has multiple GPIO modules, the DMA and the CPU can simultaneously write to the DOUTTGL register of different GPIO modules (while still requiring that the GPIO DMAMASK be configured for the GPIO module the CPU is writing to).