SLLSFV7A July 2024 – December 2025 TCAN1473A-Q1
PRODUCTION DATA
The device is designed to be a passive or no load to the CAN bus if the device is unpowered. The CANH and CANL pins have low leakage currents when the device is unpowered, thus, presenting no load to the bus. This is critical if some nodes of the network are unpowered while the rest of the of network remains in operation.
The logic terminals also have low leakage currents when the device is unpowered, so the terminals do not load down other circuits which may remain powered.