MCF8329HS read
transaction over I2C involves the following sequence (see Figure 7-55).
- I2C Start
condition from the controller to initiate the transaction.
- Start is followed by the
I2C target ID byte, made up of 7-bit target ID along with the
R/W bit set to 0b. ACK (in yellow box) indicates that MCF8329HS has processed the received target
ID which has matched with the I2C target ID and therefore
proceeds with this transaction. If target ID received does not match with
the I2C ID of MCF8329HS, then the
transaction is ignored and no ACK is sent by MCF8329HS
- The target ID byte is
followed by the 24-bit control word sent one byte at a time. Bit 23 in the
control word is set to 1b as the bit is a read transaction. ACK (in blue
boxes) correspond to acknowledgments sent by MCF8329HS to the controller that the previous byte (of control
word) has been received and next byte can be sent.
- The control word is followed
by a Repeated Start (RS, start without a preceding stop) or normal Start (P
followed by S) to initiate the data (to be read back) transfer from MCF8329HS to I2C controller. RS
or S is followed by the 7-bit target ID along with R/W bit set to 1b to
initiate the read transaction. MCF8329HS
sends an ACK (in grey box after RS) to the controller to acknowledge the
receipt of read transaction request.
- Post acknowledgment of read
transaction request, MCF8329HS sends the
data bytes on SDA one byte at a time. The number of data bytes sent by MCF8329HS depends on the DLEN field in the
control word.
- While sending data
bytes, the LSB byte is sent first. Refer to Section 7.6.2.4
for more details.
- 16-bit/32-bit Read –
The data from the address mentioned in control word is sent back to
the controller.
- 64-bit Read – 64-bit
is treated as two successive 32-bit reads. The address mentioned in
control word is taken as Addr_1. Addr_2 is internally calculated by
MCF8329HS by incrementing Addr_1
by 0x2. A total of 8 data bytes are sent by MCF8329HS. The first 4 bytes (sent in LSB first) are
read from Addr_1 and the next 4 bytes are read from Addr_2.
- ACK in orange boxes
correspond to acknowledgments sent by the controller to MCF8329HS that the previous byte has
been received and next byte can be sent.
- If CRC is enabled in the
control word, then MCF8329HS sends an additional
CRC byte at the end. Controller has to read the CRC byte and then send the
last ACK (in orange). CRC is calculated for the entire packet (Target ID + W
bit, Control Word, Target ID + R bit, Data Bytes).
- I2C Stop condition
from the controller to terminate the transaction.