SLOA332 july 2023 LMV821-N , LMV831 , OPA2991 , OPA345 , OPA376 , OPA376-Q1 , OPA377 , OPA377-Q1 , OPA4991 , OPA991 , TL074 , TLV376 , TLV9001 , TLV9002 , TS321
Most op amps do not have slew boost and slew rate. Whether an op amp has slew boost and slew rate requires assessing the listed data sheet value and the VID of the application. Boosted slew rate op amps have a more complex relationship between VID and SR. The data sheet does not always mention the presence of SR boost or the relationship with VID.
There are four methods to infer boost or no boost from a data sheet.
Section 4 describes these four methods in depth, using the data sheets for the LMV831 and TLV9001 as examples.