SLOSED5 December 2024 TRF1213
PRODUCTION DATA
TRF1213 is a wide-band, voltage-feedback amplifier with approximately 14dB of gain. When designing with a wide-band RF amplifier with relatively high gain, take precautions with board layout to maintain stability and optimized performance. Use a multilayer board to maintain signal and power integrity and thermal performance. Figure 7-6 shows an example of a good layout. This figure shows only the top layer.
Route the RF input and output lines as grounded coplanar waveguide (GCPW) lines. For the second layer, use a continuous ground layer without any ground-cuts near the amplifier area. Match the output differential lines in length to minimize phase imbalance. Use small-footprint passive components wherever possible. Also take care of the input side layout. Use a 50Ω line for the INP routing, and ensure that the termination on INM pin has low parasitics by placing the ac-coupling capacitor very close to the device. Ensure that the ground planes on the top and internal layers are well stitched with vias.
Place thermal vias under the device that connect the top thermal pad with ground planes in the inner layers of the PCB. For improved heat dissipation, connect the thermal pad to the top-layer ground plane through the ground pins (see also Section 7.4.2).