SLOU583A September   2024  – November 2024

 

  1.   1
  2.   Description
  3.   Features
  4.   4
  5. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specifications
  6. 2Quick Start Guide
    1. 2.1 Hardware Setup
    2. 2.2 Software Setup
      1. 2.2.1 Hardware Requirements
      2. 2.2.2 Software Installation
      3. 2.2.3 Launching the LIGHTSOURCE01EVM Software
      4. 2.2.4 Software Operation
        1. 2.2.4.1 LIGHTSOURCE01 GUI
    3. 2.3 LIGHTSOURCE01EVM Light Sensor Calibration
      1. 2.3.1 Mounting and Setup
      2. 2.3.2 Calibration Procedure
  7. 3Software
    1. 3.1 Scripts Window
      1. 3.1.1 Hidden IDE Window
      2. 3.1.2 devInit.py
      3. 3.1.3 mLightController.py
  8. 4Serial Commands
    1. 4.1 Latte Command Line
    2. 4.2 Terminal Application
    3. 4.3 List of Commands
  9. 5Hardware Design Files
    1. 5.1 CAD Drawings
  10. 6Compliance Information
    1. 6.1 Compliance and Certifications
  11. 7Additional Information
    1. 7.1 Troubleshooting
      1. 7.1.1 Microsoft Windows 7 Manual Driver Installation
    2. 7.2 Trademarks
  12. 8Revision History

Launching the LIGHTSOURCE01EVM Software

With the LIGHTSOURCE01EVM properly connected, launch the Latte LIGHTSOURCE01EVM GUI software from the Windows Start menu. The software launches with a screen shown in Figure 2-6.

LIGHTSOURCE01EVM LIGHTSOURCE01EVM Main
                    Operating Screen Figure 2-6 LIGHTSOURCE01EVM Main Operating Screen

If the message shown in Figure 2-7 appears when the LIGHTSOURCE01 GUI software is launched, the EVM is not detected.

LIGHTSOURCE01EVM Hardware Error Message Figure 2-7 Hardware Error Message

Check the USB connection and that the LIGHTSOURCE01EVM appears in the device manager. The EVM must occupy two COM ports: one for control and the other for data. The control port serves to send a receive the serial commands, while the data port is used for the actual transfer of data to and from the device. Refer to the following figure for an example of what the device manager must look like when connecting the device.

LIGHTSOURCE01EVM COM Ports Figure 2-8 COM Ports

If you are using Windows 7, or if the Windows device manager shows 2 USB Serial Devices under as other devices when the EVM is plugged in instead of COM ports, refer to Section 7.1.