SLPS814 November 2025 RES21A-Q1
PRODUCTION DATA
The RES21A-Q1 is typically used with two independently biased resistor dividers. RIN1 and RG1 in series form a resistive divider, with RIN2 and RG2 in series forming another divider. However, the two dividers do not have to be used independently. The resistors can be connected in series or in parallel like any other resistor.
Use one of the two GND pins to bias the part substrate. Connect the substrate to signal ground or a similar low-impedance bias point or plane for best noise rejection. While two GND/SUB connection pins are available on the device, connect only one of these to the ground plane. The two GND pins are internally connected through the substrate, which is not intended to conduct significant currents. Connect only one GND pin at a time and leave the other pin floating to prevent current return paths from developing through the substrate.