SLUAAQ0 March 2025 BQ27Z558 , BQ27Z561 , BQ27Z561-R1 , BQ27Z561-R2 , BQ27Z746 , BQ27Z758 , BQ27Z846 , BQ27Z855 , BQ28Z610 , BQ28Z610-R1 , BQ34Z100-G1 , BQ34Z100-R2 , BQ4050 , BQ40Z50 , BQ40Z50-R1 , BQ40Z50-R2 , BQ40Z80 , BQ41Z50 , BQ41Z90
BQKEYPACKAGER is intended only for an OEM to allow packaging of the authentication key. The authentication key is entered along with a password that is used in an algorithm to encrypt the file. After testing using BQKEYPROGRAMMER or BQSTUDIO, an OEM can then send the created file and password to a packmaker. Texas Instruments battery gauges have 3 methods of authentication, SHA1,SHA256, and ECC.
The output of the BQKEYPACKAGER tool is a .bqk file. This file is an encrypted output of the key generated using the tool. For the packaged .bqk file there are 2 options for output. A single file that encompasses the entire key or 2 separate files that each have one half of the key, these being part F and part C. When programming the key in production, the key can be programmed one half at a time or both halves at the same time. This allows for separate halves of the key to be programed at separate times and locations during production. For example, if you have a manufacturing flow with 2 manufacturers that the battery pack goes through. Each manufacturer can be given one half of the key to program into the gauge. This increases the security of the key as no single manufacturer has the entire key, only the OEM or designer has the key.
Figure 1-1 Split Key Production Example