SLUAB39 January 2026 BQ76905 , BQ76907 , BQ769142 , BQ76920 , BQ76930 , BQ76940 , BQ76942 , BQ76952 , BQ76972 , BQ76972-Q1
To simplify the analysis, the parasitic inductance on the load side and the battery side are equivalent to L1 and L2 respectively in the article.
Figure 2-1 shows the equivalent circuit of the low-side protection solution after DFET short-circuit protection is turned off.
After the short-circuit protection, DSG turns off. The current flowing through L1 lacks freewheeling loop, quickly reducing from Io to zero. Consequently, a substantial induced voltage is generated across L1:
and the current flowing through L2 also decreases rapidly from Io to zero because there is no freewheeling loop for the current across L2. Thus, a substantial induced voltage is also generated across L2:
Therefore, the voltage at two terminals of DS can be expressed by the following equation: