SLUSFL6D November 2024 – October 2026 TPSM82866C
PRODMIX
For most converters, the load transient response in PWM mode is improved compared to PSM, because the converter reacts faster on the load step and actively sinks energy on the load release. As an additional feature, the TPSM8286xx automatically stays in PWM mode for 128 cycles after a heavy load release to bring the output voltage back to the regulation level faster. After these 128 cycles of PWM mode, the device automatically returns to PSM (if the Enable FPWM Mode bit = 0). See Figure 7-1. Without this optimization, the output voltage overshoot is higher.